earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WorkStation, Project Configuration Server
功能: 警报, 基本功能
产品版本: 1.8
2016/10/13

Alarms Pane Shortcut Menu - Alarm View Settings Submenu

Use the Alarm View Settings submenu to change the way alarms are presented.

 
action_zoom_plus_stroke Alarm View settings submenu
图: Alarm View settings submenu

表格: Alarm View Settings Submenu

Command

Description

Display Alarm View on alarm

Click to display an Alarm View in a new window when an alarm is triggered. 有关更多信息,请参阅 Displaying an Alarm View when an Alarm is Triggered .

Edit standard filter

Click to open the Select Conditions dialog box, where you sort out the information in the Alarms pane or an Alarm View. 有关更多信息,请参阅 选择条件对话框 .

Save as standard layout

Click to save the current Alarms pane or Alarm View layout as the standard layout for all users and for the Alarms pane or the specific Alarm View.

Reset standard layout to factory default

Click to reset the Alarms pane or Alarm View standard layout to factory default.

Add/Remove columns

Click to open the Add/Remove columns dialog box to add or remove columns from the Alarms pane or Alarm View. 有关更多信息,请参阅 Add/Remove Columns Dialog Box .

Properties

Click to open the Alarm View properties dialog box to view and edit the properties of the Alarms pane or Alarm View. 有关更多信息,请参阅 Alarm View Properties .

Alarm state sort order

Click to open the Alarm state sort order dialog box to determine how alarms will be sorted when the column State is used for sorting the alarms in the Alarms pane or an Alarm View. 有关更多信息,请参阅 Determining the Alarm State Sort Order .

Detail view

Click to open a detailed view for the selected alarm. 有关更多信息,请参阅 Alarm and Event Detail View .

  • Displaying an Alarm View when an Alarm is Triggered
  • 选择条件对话框
  • Add/Remove Columns Dialog Box
  • How Alarms Work
  • Alarm View Properties
  • Determining the Alarm State Sort Order
  • Alarm and Event Detail View
  • Alarm View and Event View Standard Filter and Layout
  • Alarms Pane Shortcut Menu