earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Trendy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Zooming In an Area of a Trend Chart

You zoom in to enlarge a specific area of the trend chart to make the reading easier.

Pokaż więcej
action_close

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

You can zoom in or out on the x-axis, the y-axis, or both axes, or zoom in a specific area of the trend chart. Use the zoom to fit function to automatically adjust the trend chart x-axis and y-axis according to the range of the series displayed.

To zoom in an area of a trend chart
  1. In WebStation, in the System Tree pane, select the trend chart you want to show.

  2. Click the Zoom tool button

     
    action_zoom_plus_stroke
    .

  3. In the trend chart, select the area you want to enlarge.

  4. To zoom out, right-click in the chart.

  • Trend Chart Navigation in WebStation
  • Zooming In and Out of a Trend Chart
  • Zoom to Fit
  • Saving Current Trend Chart Settings
  • Trend Chart View