earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Trender
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Zoom to Fit

You use the zoom to fit function to resize the trend logs to fit in the browser window.

Visa mer
action_close

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

You can zoom in or out on the x-axis, the y-axis, or both axes, or zoom in a specific area of the trend chart. Use the zoom to fit function to automatically adjust the trend chart x-axis and y-axis according to the range of the series displayed.

To zoom to fit
  1. In WebStation, in the System Tree pane, select the trend chart.

  2. Click the Zoom to fit button

     
    action_zoom_plus_stroke
    .

  • Trend Chart Navigation in WebStation
  • Zooming In an Area of a Trend Chart
  • Zooming In and Out of a Trend Chart
  • Saving Current Trend Chart Settings
  • Trend Chart View