earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Zoom to Fit

You use the zoom to fit function to resize the trend logs to fit in the browser window.

显示更多
action_close

The trend chart contains a lot of tools for easy navigation in the chart. You can scroll or use the predefined settings to focus on the time span you want to see.

You can zoom in or out on the x-axis, the y-axis, or both axes, or zoom in a specific area of the trend chart. Use the zoom to fit function to automatically adjust the trend chart x-axis and y-axis according to the range of the series displayed.

To zoom to fit
  1. In WebStation, in the System Tree pane, select the trend chart.

  2. Click the Zoom to fit button

     
    action_zoom_plus_stroke
    .

  • Trend Chart Navigation in WebStation
  • Zooming In an Area of a Trend Chart
  • Zooming In and Out of a Trend Chart
  • Saving Current Trend Chart Settings
  • Trend Chart View