earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
1
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
Product version: 1.8, 1.9
5/18/2015

Logging on to WorkStation as a Building Operation User

You log on to WorkStation to securely access the functions in Building Operation.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see Licenses .

Show More
action_close

You log on to WorkStation or WebStation to securely access the functions in Building Operation.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as a Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using a Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • SmartStruxure server

To log on to WorkStation using a Windows account, you need to know the SmartStruxure server.

The account information for both the Building Operation account and the Windows account is provided by the system administrator.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see Licenses .

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • SmartStruxure server

The account information for your account is provided by the system administrator.

Remember me

For a faster log on, use the Remember me feature to automatically fill in your user name, domain, and server in both WorkStation and WebStation. For security reasons, your password is not automatically filled in. Both Building Operation users and Windows users can use the Remember me feature.

To log on to WorkStation as a Building Operation user
  1. In the User name box, type the Building Operation user name.

     
    action_zoom_plus_stroke
  2. In the Password box, type the password.

  3. In the Domain box, type a domain name. If you do not enter a domain name, you are logged on to the local domain.

  4. Select the Server hypertext transfer protocol option for communication with the SmartStruxure server.

  5. In the Server box, enter a SmartStruxure server name or an IP address.

  6. Select Remember me to have WorkStation remember your settings.

  7. Click Log on .

  8. You can register the system now or later:

    • Click Register now to register your system. For more information, see System Registration Overview .

    • Click Register later to skip registration and register at a later time.

     
    action_zoom_plus_stroke
  9. If the Select Default Workspace window is displayed, click the workspace you want to have as the default.

     
    action_zoom_plus_stroke
  • Log on to WorkStation or WebStation
  • Logging on to WorkStation using your Windows user account
  • Logging on to WorkStation as another Windows User
  • Saving Log On Details
  • Workspaces
  • Selecting a Default Workspace
  • Switching Workspaces
  • Logging Off WorkStation
  • Exiting WorkStation
  • Changing Your Password
  • Building Operation WorkStation Window
  • System Registration Overview
  • Online Registration
  • Registering an Online System
  • Offline Registration
  • Registering an Offline System