Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see Licenses .
In the User name box, type the EcoStruxure Building Operation user name.
In the Password box, type the password.
In the Domain box, type a domain name. If you do not enter a domain name, you are logged on to the local domain.
Select the Server hypertext transfer protocol option for communication with the EcoStruxure BMS server.
In the Server box, enter an EcoStruxure BMS server name or an IP address.
Select Remember me to have WorkStation remember your settings.
Click Log on .
You can register the system now or later:
Click Register now to register your system. For more information, see System Registration .
Click Register later to skip registration and register at a later time.
If the Select Default Workspace window is displayed, click the workspace you want to have as the default.