earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
03.12.2024

Editing an Extended Trend Log to be Included in Reports

You edit extended trend logs to be included in reports if you want trend log data to appear in the reports.

To edit an extended trend log to be included in reports
  1. In WorkStation, in the System Tree pane, click the extended trend log you want to include in reports.

  2. In the Extended Trend Log properties, in the Include in Reports box, select True .

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

The extended trend log is set up to be included in reports.

  • Configuring an Extended Trend Log
  • Extended Trend Log Properties – Basic Tab
  • Extended Trend Logs