功能: 趋势
产品版本: 1.8
2016/10/13

Editing an Extended Trend Log to be Included in Reports

You edit extended trend logs to be included in reports if you want trend log data to appear in the reports.

显示更多
action_close

报告可在 WorkStation 或 Web 浏览器中查看。如要查看报告,您需要一个 WorkStation 用户帐户。当您登录在 WorkStation 或 Web 浏览器中查看报告时,需要使用您的 WorkStation 用户名和密码。

To edit an extended trend log to be included in reports
  1. In WorkStation, in the System Tree pane, click the extended trend log you want to include in reports.

  2. In the Include in Reports box, select True .

     
    action_zoom_plus_stroke
  3. Click the Save button

     
    action_zoom_plus_stroke
    .

The extended trend log is set up to be included in reports.

  • Configuring an Extended Trend Log
  • Extended Trend Log Properties
  • Extended Trend Logs
  • 报告运作方式