earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebHelp
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2021-08-27

Subscriptions

You can subscribe to and receive notifications by E-mail when the following WebHelp events occur:

  • A WebHelp topic is published or updated

  • Community content for a topic is added or edited

If you subscribe to topic updates, the subscription checks for changes that are made for a specific language. For example, if you subscribe to topics that are published in English, you do not receive E-mail notifications when Danish topics are updated. You receive a notification once a day. The E-mail contains links to all topics that have been published or updated during the day.

If you subscribe to all community content updates, you receive a notification once a day. The E-mail contains links to community content that other users have added or edited during the day. When you add or edit community content for a topic, WebHelp creates a thread to the community content and activates a subscription for updates for the thread. This subscription means that you directly receive E-mail notifications when other users add or edit information in the community content.

You need to log on to WebHelp to subscribe to the WebHelp events.

  • Features
  • WebHelp Overview
  • Log on
  • WebHelp Subscribe to Updates Page
  • Subscribing to Topic and Community Content Updates
  • Unsubscribing from Topic and Community Content Updates
  • Unsubscribing from a Community Content Thread