earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Especificaciones

Especificaciones


Productos Enterprise Server
Funcionalidades: Ingeniería
Versión del producto: 2024
20/12/2024

Enterprise Server

arrow1_rotationIntroducción arrow1_rotationCaracterísticas arrow1_rotationEspecificaciones
 
action_zoom_plus_stroke Enterprise Server
Figura: Enterprise Server

Introducción

Un servidor EcoStruxure BMS es el núcleo del sistema y realiza funciones clave, como la lógica de control, el registro de tendencias y la supervisión de alarmas. Enterprise Server recopila datos de todas las instalaciones para agregarlos y archivarlos, y sirve como punto único de administración a través de WorkStation o WebStation para el EcoStruxure BMS, el sistema inteligente de gestión de edificios de Schneider Electric.

Características

El servidor Enterprise Server es el punto central en la arquitectura de EcoStruxture BMS, desde el que los usuarios pueden configurar, controlar y supervisar todo el sistema.

Semantics

Enterprise Server and Enterprise Central come with built-in support for modelling of the “digital twin” of the building, site, campus, and region using Brick Schema. WorkStation and WebStation provide enhanced human understandability through the additional context that is given to alarms and points through the “digital twin”. The required graph database is included in the installation packages. WorkStation can be used to create the model, or it can be imported using the graph database user interface.

El poder de las redes

El servidor Enterprise Server puede ejecutar varios programas de control usando distintos protocolos. Puede gestionar alarmas, usuarios, planificaciones y registros de tendencias. Los datos se pueden enviar directamente desde Enterprise Server al usuario o a otros dispositivos de campo y servidores EcoStruxure de la instalación o la empresa.

Global view of the system

The entire site, including all of the field servers and their associated devices, can be accessed and configured through the Enterprise Server.

This overview of the site provides easier mass change engineering and data analysis. The Enterprise Server also aggregates the event and alarm data from all its associated field servers. Trend logs can be aggregated through the use of extended trend logs.

Text and graphics-based programming tools

Unique to the industry, the EcoStruxure BMS servers have both Script and Function Block programming options. This flexibility helps assure that a suitable programming method can be selected for the application.

Centralized alarms and data management

Alarms from multiple devices throughout the site, including field servers, are collected by the Enterprise Server for centralized logging, display, and management. Users can also view event logs and trend logs from multiple servers.

The Enterprise Server hosts the historical and configuration databases. These databases store current information, including trends, alarms, user activity, and property information. Alarms can trigger email, SNMP, file, or client notifications, which can include alarm, point value, or trend log data. Notifications can also be triggered periodically by schedules or other binary values.

EcoStruxure BMS servers can be configured to automatically store all historical data, trend log data, event log and audit trail data, in an external database. If data needs to be available for longer periods of time, an external log storage can be incorporated into the EcoStruxure BMS without the need for extensive engineering work. The supported databases are TimescaleDB, which is built on PostgreSQL, and Microsoft SQL Server. The data in the external log storage is available natively to the viewers built into the EcoStruxure Building Operation clients and to the built-in reporting functionality.

You can use the powerful Log Processor functionality for custom processing of trend data for viewing in charts, dashboards and for inclusion in reports. The Log Processor enables advanced calculations on one or multiple trend logs and point values.

Examples of advanced calculations:

  • Energy usage normalization

  • Virtual submeters and summaries

  • Calculation of Mean Kinetic Temperature

  • Unit conversions

  • Average, maximum, and mini m um over custom periods

The output of the Log Processor can be saved in the database, including the External Log Storage or calculated automatically on demand.

Selected trend logs and the event log can be sent to AVEVA PI System directly without the need for intermediate storage or specialized PI System connectors.

Reporting

The EcoStruxure BMS servers provide built-in functionality for basic reporting that can deliver reports in any text format and XLSX, without any dependencies to other external software. Reports for XLSX can be enriched by using advanced functionality such as formulas, conditional formatting, charts and sparklines.

Reports can be generated on schedule, on an alarm event or other custom conditions, and you can get the output delivered via email or written to file.

Using Enterprise Server and Enterprise Central, reports can be converted to PDF, and you can elevate the data security and traceability even further by using the optional add-on for automatically signing PDF reports with a digital certificate upon generation. This validates that the content has not been altered after the report was generated.

Authentication and permissions

An EcoStruxure BMS provides a powerful permission system that is easy to manage, flexible, and adapts to all kinds of system sizes. The permission system provides a high standard of authentication. Authentication is done against the built-in user account management system , against Windows Active Directory Domains , or via SAML 2.0 single sign-on . The built-in account management system allows an administrator to establish password policies that meet stringent cybersecurity guidelines. When Windows Active Directory or SAML 2.0 authentication is used, the administration costs are lower because users do not have to be managed in multiple directories.

Registro de actividades avanzadas

Es importante registrar algo más que las actividades básicas. En una solución EcoStruxure BMS, cada acción se registra con una marca de tiempo, el usuario que la ha realizado y los valores que se han cambiado.

WorkStation/WebStation interface

Through any client, the user experience is similar regardless of which EcoStruxure BMS server the user is logged on to. The user can log directly on to an Enterprise Server to engineer, commission, supervise, and monitor the field servers with their attached Central IO modules, field controllers, and other field devices. For more information, see the WorkStation and WebStation specification sheets.

Conectividad con protocolos abiertos para la gestión energética de edificios

Una de las principales características de la solución EcoStruxure BMS es su compatibilidad con los estándares abiertos. Enterprise Server puede comunicarse de forma nativa con algunos de los estándares más populares para edificios: BACnet (incluido BACnet/SC), OPC UA Client, LonWorks y Modbus.

Compatibilidad nativa con BACnet catalogada por BTL

El servidor Enterprise Server se comunica directamente con las redes BACnet/IP. El servidor Enterprise Server está catalogado por BTL como un controlador BACnet para la gestión energética de edificios (B-BC), el perfil de dispositivo BACnet más avanzado, y como BACnet Operator Workstation (B-OWS). Esta funcionalidad permite acceder a toda la gama de dispositivos BACnet de Schneider Electric y otros proveedores. Consulte en el catálogo de productos de BTL los detalles actualizados de las revisiones de software incluidas por BTL en la página de BACnet International. El servidor Enterprise Server también puede actuar como un dispositivo de gestión de transmisión BACnet (BBMD) para que los sistemas BACnet puedan llegar a varias subredes IP.

BACnet/SC (Secure Connect) support

The Enterprise Server and field servers support BACnet/SC applications as a BACnet/SC node, hub, and router. This allows the Enterprise Server and field servers to be in BACnet/SC networks and support applications that connect BACnet/IP or MS/TP networks with BACnet/SC networks. A major benefit of BACnet/SC is that it allows more secure transport of BACnet traffic and information between BACnet/SC devices over private and public networks without the need for BBMDs, VLANs, and VPNs, because the BACnet/SC protocol uses WebSocket technology and TLS 1.3 encryption. In addition, BACnet/SC uses certificate management to help ensure only those devices authorized to be on a BACnet/SC network can operate on that network.

Native OPC UA Client support

OPC UA Client functionality is natively supported in Enterprise Server and field servers, enabling powerful and high-capacity integration of devices or systems that have OPC UA Server capability. OPC Unified Architecture (OPC UA) is a standard originating from industrial automation and process control that provides methods intended to provide improved security, performance, and engineering efficiency. With OPC UA Client support, the EcoStruxure Building Operation software can monitor and control a wide variety of devices or systems, from Schneider Electric as well as from other companies.

Compatibilidad nativa con LonWorks

El servidor Enterprise Server funciona con toda una gama de adaptadores LonTalk para comunicarse con redes TP/FT-10 LonWorks. La funcionalidad LonWorks integrada permite acceder a los dispositivos LonWorks de Schneider Electric y otros proveedores. Las redes LonWorks pueden ponerse en marcha, vincularse y configurarse desde el servidor Enterprise Server usando la herramienta de gestión de redes LonWorks integrada. No se necesitan herramientas de terceros. Para una mayor facilidad de uso, se admiten los plugins de dispositivos LNS. Esto facilita las tareas de ingeniería y mantenimiento de los dispositivos LonWorks de Schneider Electric y otros proveedores. Hay algunas limitaciones respecto al uso de los plugins de dispositivos LNS.

Native Modbus support

The Enterprise Server and field servers natively integrate Modbus RS-485 client and server configurations, as well as Modbus TCP client and server. This allows full access to third-party products and the range of Schneider Electric products that communicate on the Modbus protocol, such as power meters, UPS, circuit breakers, lighting controllers, and emergency lighting.

Modbus device types are pre-configured Modbus applications for quick and easy Modbus device integration in EcoStruxure Building Operation solutions.

Compatibilidad con servicios web

El servidor Enterprise Server es compatible con el uso de servicios web basados en estándares abiertos, como SOAP y REST, para usar los datos en la solución EcoStruxure BMS. Use los datos de terceros (previsión de temperaturas, costes energéticos) disponibles en la web para determinar los modos de la instalación, la planificación y programación.

EcoStruxure Web Services support

EcoStruxure Web Services, Schneider Electric’s Web Services standard, is natively supported in the EcoStruxure BMS servers. EcoStruxure Web Services offers extra features between compliant systems whether within Schneider Electric or other authorized systems. These features include access to semantic model, system directory browsing, read/write of current values, alarm receipt and acknowledgement, and historical trend log data. EcoStruxure Web Services requires user name and password to log on to the system.

MQTT IoT protocol support

The Enterprise Server and field servers support MQTT as an option for publishing data to, and receiving updates from, other systems. MQTT is a messaging transport protocol that with its small footprint, light bandwidth utilization, and simplicity, is ideal for M2M and IoT communication. The MQTT capability supports communication with any MQTT broker, for example, Amazon, Microsoft, Google or IBM.

IT friendly

The EcoStruxure BMS servers communicate using the networking standards. This makes installations easy, management simple, and transactions more secure.

Protocolos compatibles
  • Dirección IP

  • Comunicaciones TCP

  • Fácil configuración con DHCP

  • El DNS permite acceder a direcciones de forma simple

  • HTTP/HTTPS para el acceso a Internet a través de firewalls, lo que permite el control y la supervisión remotos

  • NTP (protocolo de tiempo de red) para la sincronización de la hora en todo el sistema

  • SMTP/SMTPS con soporte para autenticación basada en SSL/TLS, permite el envío de mensajes de correo electrónico desencadenados por un calendario o alarma

  • SNMP permite recibir alarmas de aplicaciones en herramientas de gestión de redes específicamente diseñadas.

  • Cifrado WebSocket Secure (WSS) y TLS 1.3 (aplicaciones BACnet/SC)

TLS support

Communication between clients and the EcoStruxure BMS servers , and between EcoStruxure BMS servers, can be encrypted using Transport Layer Security (TLS ). The servers are delivered with a default self-signed certificate. Commercial Certification Authority (CA) server certificates are supported to lower the risk of malicious information technology attacks. Use of encrypted communication can be enforced for both WorkStation and WebStation access.

Tabla: Automatización de edificios – Disponibilidad de licencias para Windows y Linux

Licencias de Enterprise Server

Ventanas

Linux

Enterprise Server - 10 servidores de automatización a

Enterprise Server - 50 servidores de automatización a

Enterprise Server - 100 servidores de automatización a

Enterprise Server - 250 servidores de automatización a

  1. Para más información sobre los números de referencia, consulte la subsección “Números de referencia” de la sección “Especificaciones”.

Actualizar las licencias del paquete de software

Ventanas

Linux

Actualización 3.x - 10 servidores de automatización a

-

Actualización 3.x - 50 servidores de automatización a

-

Actualización 3.x - 100 servidores de automatización a

-

Actualización 3.x - 250 servidores de automatización a

-

Actualización 4.x o 5.x - 10 servidores de automatización a

-

Actualización 4.x o 5.x - 50 servidores de automatización a

-

Actualización 4.x o 5.x - 100 servidores de automatización a

-

Actualización 4.x o 5.x - 250 servidores de automatización a

-

  1. Para más información sobre los paquetes de software de actualización, consulte la subsección “Paquetes de software de actualización” de la sección “Especificaciones”.

Licencias opcionales de complementos

Ventanas

Linux

Paquete ES Hosting AS - 01 a

Paquete ES Hosting AS - 10 a

Paquete ES Hosting AS - 50 a

Paquete ES Hosted Node - 5 a

Paquete ES Hosted Node - 10 a

Paquete ES Hosted Node - 25 a

Paquete ES Hosted Node - 50 a

Paquete ES Hosted Node - 100 a

Paquete ES Hosted Node - 300 a

Paquete ES Hosted Node - 600 a

Consumo de EcoStruxure Web Services a

Servicios y consumo de EcoStruxure EcoStruxure Web Services a

Servicio y consumode EcoStruxure Web Services y datos de registro de tendencias históricas a

Servicios web opcionales (consumo genérico) a

Notificaciones opcionales de alarmas a través de SNMP a

Licencia de implementación del conector inteligente a

-

Paneles personales opcionales a

Conexión TimescaleDB opcional a

Conexión opcional a Microsoft SQL Server a

Conexión opcional al sistema AVEVA PI a

Paquete de cumplimiento de industrias reguladas opcional a

Firma de PDF opcional a

MQTT opcional a

Zonificación opcional a

Autenticación SAML opcional a

Semantic DB Plus 2 núcleos de CPU a

-

Semantic DB Plus 6 núcleos de CPU a

-

Semantic DB External Use Plus 2 núcleos de CPU a

-

Semantic DB External Use Plus 6 núcleos de CPU a

-

Paquete de sostenibilidad opcional a

Cliente OPC UA opcional a

  1. Para más información sobre las opciones adicionales, consulte la subsección “Opciones adicionales” de la sección “Especificaciones”.

Tabla: Fire Detection – Windows and Linux Licences Availablility

Enterprise Server Licenses

Windows

Linux

Enterprise Server 1 year on premise subscription duration a

Yes

-

Essential plan 1 year on premise subscription duration Enterprise Server a

Yes

-

Enhanced plan 1 year on premise subscription duration Enterprise Server a

Yes

-

Advanced plan 1 year on premise subscription duration Enterprise Server a

Yes

-

  1. For more information on the part numbers, see section “Specifications”, subsection “Part Numbers”.

Add-on Option Licences

Windows

Linux

Connected Device on premise 1 year 10-pack, EcoStruxure Building Operation a

Yes

-

  1. For more information on the add-on options, see section “Specifications”, subsection “Add-on options”.

Especificaciones

Hardware requirements
Processor power, memory, and storage capacity should be scaled upwards to accommodate targeted system size as impacted by the total quantity of automation servers and expected historical archiving. Enterprise Server is tested on many different servers with varying configurations. The typical configuration is an 8-core 3.6 GHz processor, 32 GB of memory, and SSD storage capacity of 1 TB.
Processor
Minimum: Intel Core i5 @ 2.0 GHz or equivalent
  
Recommended: Intel Core i5 @ 3.0 GHz or better
Memory
Minimum: 8 GB
  
Recommended: 16 GB or higher
Storage capacity
Minimum: 100 GB
  
Recommended: 1 TB
Storage device
Recommended: Enterprise Solid State Drive (SSD)
An Enterprise SSD is recommended to maintain the necessary speed and stability. The database and the binaries should both be installed on the Enterprise SSD.
Other devices
Microsoft mouse or compatible pointing device is required.
Software requirements
Operating systems – Enterprise Server for Windows
Microsoft Windows 10 (64-bit)
  
Microsoft Windows 11 a
  
Microsoft Windows Server 2012 R2 (64-bit)
  
Microsoft Windows Server 2016
  
Microsoft Windows Server 2019
  
Microsoft Windows Server 2022 a
The following Microsoft Windows 10 editions are supported: Pro and Enterprise.
The following Microsoft Windows 11 a editions are supported: Pro and Enterprise.
The following Microsoft Windows Server 2012 R2 editions are supported: Datacenter, Standard, Essentials, and Foundation.
The following Microsoft Windows Server 2016 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2019 editions are supported: Datacenter, Standard, and Essentials.
The following Microsoft Windows Server 2022 a editions are supported: Datacenter, Standard, and Essentials.
Operating systems – Enterprise Server for Linux
OCI compliant container runtime on Linux x86-64
Quality assurance testing has been performed on, and support is provided with, Ubuntu 20.04 and 22.04 with Docker Engine version 20.10.00. Other deployment scenarios have not been tested by Schneider Electric. Product Support Services may require that potential issues can be reproduced in tested and supported environment for full support.
Required additional software – Enterprise Server for Windows
Microsoft .NET Framework 4.7.2 and later
The Microsoft .NET Framework is required by Software Administrator.
External log storage PostgreSQL option
Supported versions of PostgreSQL ( www.postgresql.org ) with matching version of TimescaleDB extension ( www.timescale.com ).
  
Note: To use compression for trend data, TimescaleDB 2.11 or later is required.
Quality assurance testing has been performed by Schneider Electric with TimescaleDB and PostgreSQL installed natively in Windows 10, Windows Server 2012, 2016, and 2019. Other deployment scenarios have not been tested by Schneider Electric.
External log storage Microsoft SQL option
Microsoft SQL Server versions under full support by Microsoft ( www.microsoft.com ).
The following Microsoft SQL Server editions are supported: Enterprise, Standard, and Express.
External log storage AVEVA PI System option
PI Web API 2021 SP3 and database compatible with that version
Quality assurance testing has been performed by Schneider Electric with PI Web API 2021 SP3, and database compatible with that version, installed on Windows Server 2019. Other deployment scenarios have not been tested by Schneider Electric.
Communication
TCP
Binary, port fixed, 4444
HTTP
Non-binary, port configurable, default 80
HTTPS
Encrypted supporting TLS 1.3, 1.2, 1.1 a , and 1.0 a , port configurable default 443
WSS a
Encrypted supporting TLS 1.3, port configurable
SMTP
Email sending, port configurable, default 25
SMTPS
Email sending, port configurable, default 587
SNMP
version 3
  
Application alarm distribution using trap
NTP
Time synchronization
BACnet
BACnet/IP, port configurable, default 47808
  
BACnet/SC, port configurable, no default port
  
BTL B-BC (BACnet Building Controller) a
  
BTL B-SCHUB (BACnet Secure Connect Hub) a
  
BTL B-OWS (BACnet Operator Workstation) a
OPC UA Client
Profile group UACore 1.03
Core Client Facet, Base Client Behaviour Facet a , AddressSpace Lookup Client Facet, Attribute Read Client Facet a , Attribute Write Client Facet a , DataChange Subscriber Client Facet a , Method Client Facet, UA-TCP UA-SC UA-Binary, SecurityPolicy – Basic256, SecurityPolicy – Basic256Sha256, User Token – Anonymous Facet, User Token – User Name Password Client Facet, DataAccess Client Facet, Base Event Processing Client Facet, and Historical Access Client Facet.
Modbus
Modbus TCP, client and server
  
Modbus RTU and ASCII, RS-485, client and server a
MQTT
MQTT over TLS, port configurable, default 8883
  
MQTT over TCP, port configurable, default 1883
  
MQTT over WebSocket Secure (WSS), port configurable, default 443
  
MQTT over WebSocket (WS), port configurable, default 80
Supports the following LonTalk adapters:
NIC709-PCI
  
NIC709-USB
  
NIC709-USB100
  
NIC709-IP
  
NIC852
Se pueden usar otros protocolos para funciones concretas adicionales. Consulte la documentación técnica.
LNS
Versión LNS
OpenLNS
Instalado en un PC WorkStation
LonMark
Resource files version
14.00
Part numbers
Building Automation – Enterprise Server for Windows
Enterprise Server - 10, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 10 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00010
Enterprise Server - 50, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 50 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00050
Enterprise Server - 100, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 100 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00100
Enterprise Server - 250, EcoStruxure Building Operation Enterprise Server license for a PC server, includes support for 250 automation servers , 3 concurrent clients , and 1 semantic database limited to 2 CPU cores
SXWSWESXX00250
Building Automation – Enterprise Server for Linux
Enterprise Server - 10, licencia de EcoStruxure Building Operation Enterprise Server para Linux, incluye soporte para 10 servidores de automatización y 3 clientes simultáneos
SXWSWESLX00010
Enterprise Server - 50, licencia de EcoStruxure Building Operation Enterprise Server para Linux, incluye soporte para 50 servidores de automatización y 3 clientes simultáneos
SXWSWESLX00050
Enterprise Server - 100, licencia de EcoStruxure Building Operation Enterprise Server para Linux, incluye soporte para 100 servidores de automatización y 3 clientes simultáneos
SXWSWESLX00100
Enterprise Server - 250, licencia de EcoStruxure Building Operation Enterprise Server para Linux, incluye soporte para 250 servidores de automatización y 3 clientes simultáneos
SXWSWESLX00250
Fire Detection – Enterprise Server for Windows
Enterprise Server 1 year on premise subscription duration
FFSEFOSES00012
Essential plan 1 year on premise subscription duration Enterprise Server
FFSEFOPES00112
Enhanced plan 1 year on premise subscription duration Enterprise Server
FFSEFOPEH00112
Advanced plan 1 year on premise subscription duration Enterprise Server
FFSEFOPAD00112
Upgrade software bundles
Building Automation – Enterprise Server for Windows
Enterprise Server Upgrade – 10 or fewer automation servers
Upgrades Enterprise Server, with 10 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30010
Enterprise Server Upgrade – 50 or fewer automation servers
Upgrades Enterprise Server, with 50 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30050
Enterprise Server Upgrade – 100 or fewer automation servers
Upgrades Enterprise Server, with 100 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30100
Enterprise Server Upgrade – 250 or fewer automation servers
Upgrades Enterprise Server, with 250 or fewer hosted automation servers, from EcoStruxure Building Operation software version 3.x to 6.0.
SXWSWESUP30250
Enterprise Server Upgrade – 10 or fewer automation servers
Upgrades Enterprise Server, with 10 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40010
Enterprise Server Upgrade – 50 or fewer automation servers
Upgrades Enterprise Server, with 50 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40050
Enterprise Server Upgrade – 100 or fewer automation servers
Upgrades Enterprise Server, with 100 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40100
Enterprise Server Upgrade – 250 or fewer automation servers
Upgrades Enterprise Server, with 250 or fewer hosted automation servers, from EcoStruxure Building Operation software version 4.x or 5.x to 6.0.
SXWSWESUP40250
Add-on options
Building Automation – Enterprise Server for Windows
ES Hosting AS Pack - 01, License to add 1 automation server
in addition to the original Enterprise Server purchased size.
SXWSWASES00001
ES Hosting AS Pack - 10, License to add 10 automation servers
in addition to the original Enterprise Server purchased size.
SXWSWASES00010
ES Hosting AS Pack - 50, License to add 50 automation servers
in addition to the original Enterprise Server purchased size.
SXWSWASES00050
ES Hosted Node Pack - 5, License to add 5 Non-SpaceLogic servers/controllers.
SXWSWNDES00005
ES Hosted Node Pack - 10, License to add 10 Non-SpaceLogic servers/controllers.
SXWSWNDES00010
ES Hosted Node Pack - 25, License to add 25 Non-SpaceLogic servers/controllers.
SXWSWNDES00025
ES Hosted Node Pack - 50, License to add 50 Non-SpaceLogic servers/controllers.
SXWSWNDES00050
ES Hosted Node Pack - 100, License to add 100 Non-SpaceLogic servers/controllers.
SXWSWNDES00100
ES Hosted Node Pack - 300, License to add 300 Non-SpaceLogic servers/controllers.
SXWSWNDES00300
ES Hosted Node Pack - 600, License to add 600 Non-SpaceLogic servers/controllers.
SXWSWNDES00600
SW-EWS-1, EcoStruxure Web Services (run-time) option
Consume only for one Enterprise Server or one Enterprise Central
SXWSWEWSX00001
SW-EWS-2, EcoStruxure Web Services (run-time) option
Serve & Consume for one Enterprise Server or one Enterprise Central
SXWSWEWSX00002
SW-EWS-3, EcoStruxure Web Services (run-time) option
Serve & Consume, plus Historical trend log data for one Enterprise Server or one Enterprise Central
SXWSWEWSX00003
SW-GWS-1, Web Services (Generic Consume) option
For one Enterprise Server or one Enterprise Central
SXWSWGWSX00001
SW-SNMP-1, Alarm notifications via SNMP option
For one Enterprise Server or one Enterprise Central
SXWSWSNMP00001*
SW-SMART-CONNECT, Smart Connector deployment license
For one Smart Connector deployment
SXWSWSCDL100001
Building Operation Personal Dashboards option, 1 per server required for users logging on to that server to have Personal Dashboard capabilities
For one Enterprise Server or one Enterprise Central
SXWSWDASH00001
SW-ESDBTS-1, TimescaleDB connection option
For one Enterprise Server
SXWSWESDBTS001*
EcoStruxure Building Operation, Microsoft SQL Server connection option
For one Enterprise Server
SXWSWESDBMS001*
EcoStruxure Building Operation, AVEVA PI System connection option
For one Enterprise Server
SXWSWESDBPI001*
Regulated Industries Compliance Pack option
For one Enterprise Server or one Enterprise Central
SXWSWCMPLPK001*
SW-ESPDF-1, opción dde firma de PDF de Building Operation
Para un Enterprise Server
SXWSWESPDFSS01
SW-ESMQTT-1, MQTT option
For one Enterprise Server
SXWSWMQTTSRW01*
Building Operation Zoning option
For one Enterprise Server
SXWSWESSDZR001
SAML Authentication option
For one Enterprise Server
SXWSWESSAML001*
Semantic DB Plus 2 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC002
Semantic DB Plus 6 CPU Cores
Additional concurrent queries for one semantic database
SXWSWSTDBAC006
Semantic DB External Use Plus 2 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC2
Semantic DB External Use Plus 6 CPU Cores
Enables queries from external tools and additional concurrent queries
SXWSWSTDBEUAC6
Sustainability Pack option
For one Enterprise Server for Windows
SXWSWESSUSPKW1*
OPC UA Client option
For one Enterprise Server for Windows
SXWSWESOPCLW01*
Building Automation – Enterprise Server for Linux
Paquete ES Linux Hosting AS - 01, Licencia para añadir 1 servidor de automatización
además del tamaño original de Enterprise Server para Linux comprado.
SXWSWASESL0001
Paquete ES Linux Hosting AS - 10, Licencia para añadir 10 servidores de automatización
además del tamaño original de Enterprise Server para Linux comprado.
SXWSWASESL0010
Paquete ES Linux Hosting AS - 50, Licencia para añadir 50 servidores de automatización
además del tamaño original de Enterprise Server para Linux comprado.
SXWSWASESL0050
Paquete ES Linux Hosted Node - 5, Licencia para añadir 5 servidores/controladores no SpaceLogic.
SXWSWNDESL0005
Paquete ES Linux Hosted Node - 10, Licencia para añadir 10 servidores/controladores no SpaceLogic.
SXWSWNDESL0010
Paquete ES Linux Hosted Node - 25, Licencia para añadir 25 servidores/controladores no SpaceLogic.
SXWSWNDESL0025
Paquete ES Linux Hosted Node - 50, Licencia para añadir 50 servidores/controladores no SpaceLogic.
SXWSWNDESL0050
Paquete ES Linux Hosted Node - 100, Licencia para añadir 100 servidores/controladores no SpaceLogic.
SXWSWNDESL0100
Paquete ES Linux Hosted Node - 300, Licencia para añadir 300 servidores/controladores no SpaceLogic.
SXWSWNDESL0300
Paquete ES Linux Hosted Node - 600, Licencia para añadir 600 servidores/controladores no SpaceLogic.
SXWSWNDESL0600
EcoStruxure Web Services ( tiempo de ejecución) opcional
Consumo solo para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWEWSL00001
EcoStruxure Web Services ( tiempo de ejecución) opcional
Servicio y consumo para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWEWSL00002
EcoStruxure Web Services ( tiempo de ejecución) opcional
Servicio y consumo, además de datos de registro de tendencias históricas para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWEWSL00003
Servicios Web ( consumo genérico) opcional
Para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWGWSL00001
Notificaciones de alarma a través de SNMP opcionales
Para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWSNMPL0001
Paneles personales opcionales, se requiere 1 por servidor para que los usuarios que inicien sesión en ese servidor dispongan de capacidades de panel personal
Para un Enterprise Server para Linux o un Enterprise Central para Linux
SXWSWDASHL0001
Conexión TimescaleDB opcional
Para un Enterprise Server para Linux
SXWSWESDBTSL01*
Conexión opcional a Microsoft SQL Server
Para un Enterprise Server para Linux
SXWSWESDBMSL01*
Conexión opcional al sistema AVEVA PI
Para un Enterprise Server para Linux
SXWSWESDBPIL01*
Regulated Industries Compliance Pack option
For one Enterprise Server for Linux or one Enterprise Central for Linux
SXWSWCMPLPKL01*
Firma de PDF opcional
Para un Enterprise Server para Linux
SXWSWESPDFSSL1
MQTT opcional
Para un Enterprise Server para Linux
SXWSWMQTTSRWL1*
Opción de zonificación
Para un Enterprise Server para Linux
SXWSWESSDZRL01
Opción de autenticación SAML
Para un Enterprise Server para Linux
SXWSWESSAMLL01*
Sustainability Pack option
For one Enterprise Server for Linux
SXWSWESSUSPKL1*
OPC UA Client option
For one Enterprise Server for Linux
SXWSWESOPCLL01*
Fire Detection – Enterprise Server for Windows
Connected Device on premise 1 year 10-pack, EcoStruxure Building Operation
FFSEFOCDE00112