earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: WebReports
Funktionen: Berichte
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16.12.2021

Energy Monitoring Consumption Breakdown Report

The Energy Monitoring Consumption Breakdown report displays a pie chart that shows the relative cost, units, and CO 2 consumption between different power meters. You can use the report to compare energy usage between power meters.

The following table shows the input parameters for the report.

Tabelle: Energy Monitoring Consumption Breakdown Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time for reporting on the energy consumption.

End report date/time

Specifies the end date and time for reporting on the energy consumption.

Utility type

Specifies the type of utility (gas, electricity, or meter).

Power meter

Specifies the meter or site included in the report.

Date filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

CO2 tonnes per unit

Specifies the carbon tonnage per unit.

Cost per unit

Specifies the cost per unit.

Currency

Specifies the currency to be used to calculate the consumption cost.

  • Factory Supplied Reports
  • Energy Monitoring Reports
  • Creating the Energy Folder
  • Creating a Site
  • Configuring a Site
  • Creating a Meter
  • Configuring a Meter
  • Associating an Extended Trend Log with an Energy Meter
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Attaching an Existing Tag to an Energy Object
  • Deleting an Energy Object Tag
  • Site Properties – Basic Tab
  • Energy Folder Properties – Basic Tab
  • Electricity Meter Properties – Basic Tab
  • Gas Meter Properties – Basic Tab
  • Meter Properties – Basic Tab