earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
Interface de utilizador

Interface de utilizador


Produtos: WebReports
Funcionalidades: Relatórios
Versão do produto: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16-12-2021

Electricity Meter Properties – Basic Tab

Use the ​ Basic tab to enter meter numbers, associate the meter with an extended trend log, and to add or remove tags.

 
action_zoom_plus_stroke Basic tab
Imagem: Basic tab

Tabela: Basic Tab

Property

Description

Utility

Displays the utility selected on creation of the meter.

Meter Reference Number

Type the meter reference number.

Meter Serial Number

Type the meter serial number.

Meter Trend Log

Enter the path of the extended trend log you want to associate with this meter.

Attached tags

Displays all tags attached to the energy object.

Enter a new tag

Type the text you want to be displayed in a new tag.

 
action_zoom_plus_stroke

Click to place a new tag in the Attached tags area after you have entered text in the Enter a new tag box.

 
action_zoom_plus_stroke

Click to open the Add Existing Tags dialog box. Para mais informações, consulte Add Existing Tags Dialog Box .

  • General Information Properties – Basic Tab
  • Energy Monitoring Reports
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Add Existing Tags Dialog Box