earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Gas Meter Properties – Basic Tab

Use the ​ Basic tab to enter the meter reference numbers, associate the meter with an extended trend log, and to add or remove tags.

 
action_zoom_plus_stroke Basic tab
图: Basic tab

表格: Basic Tab

Property

Description

Utility

Displays the utility selected on creation of the meter.

Meter Reference Number

Type the meter reference number.

Meter Serial Number

Type the meter serial number.

Meter Trend Log

Enter the path of the extended trend log you want to associate with this meter.

Attached tags

Displays all tags attached to the energy object.

Enter a new tag

Type the text you want to be displayed in a new tag.

 
action_zoom_plus_stroke

Click to place a new tag in the Attached tags area after you have entered text in the Enter a new tag box.

 
action_zoom_plus_stroke

Click to open the Add Existing Tags dialog box. 有关更多信息,请参阅 Add Existing Tags Dialog Box .

  • General Information Properties – Basic Tab
  • Energy Monitoring Reports
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Add Existing Tags Dialog Box