Retain level is a property of a variable that determines the variables persistence during restarts. This is important for saving user-configured values or specific application data that should survive a reboot.
Variable values are stored in the following way:
Flash memory is used to store most variable values, so they survive power failures and server shutdowns.
SDRAM, that is a temporary memory, is used for frequently collected values to avoid wearing out the flash memory.
All variable has a retain level that can be configured by the user. The retain level controls if the value of the variable is retained after a restart. The retain levels affect:
Whether the value is kept after a cold start or warm start
Whether the value is saved in the configuration database
The default setting for retain level in the variable is Warm start.
|
Restart mode |
Retain level configured by user:
No |
Retain level configured by user: Warm start |
Retain level configured by user: Cold start |
|
Warm start |
Values configured by a user or application are lost. |
Variable retains last value configured by a user. Values configured by an application are retained. |
Variable retains last value configured by a user. Values configured by an application are retained. |
|
Cold start |
Values configured by a user or application are lost. |
Variable loses last value configured by a user. Values configured by an application are lost. |
Variable retains last value configured by a user. Values configured by an application are retained. |
|
System Events and Activities |
Initiated from |
System response |
Variable retain level |
|
Warm start command |
WorkStation |
Application restarts |
Warm start |
|
Cold start command |
WorkStation |
Application restarts |
Cold start |
|
Restart command |
Device Administrator |
Full device restart |
Warm start |
|
Power fail |
X |
Full device restart |
Warm start |
|
Restore (from a backup) |
WorkStation |
Application restarts |
Warm start |
|
Upgrade |
WorkStation |
Full device restart |
Warm start |
|
Exporting & Importing |
WorkStation |
Application restarts |
Warm start |
|
Reset button |
One short push on Reset button on field server. |
Full device restart |
Warm start |
Function block objects have their own backup function. The backup function in Function Block overrides the retain level in EcoStruxure BMS for a warm start. Para obtener más información, consulte Function Block Program - Retain Versus Backup .