earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: WebStation
Funzionalità: Programmi orari
Versione del prodotto: 1.8
10/06/2016

Xenta Schedules in WebStation

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. You can assign and unassign lead Xenta central schedules. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

Per maggior informazioni, consulta Come funzionano i programmi orari .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

Per maggior informazioni, consulta Xenta Central Schedules .

  • Come funzionano i programmi orari
  • Adding a Weekly Event to a Xenta Schedule in WebStation
  • Adding an Exception Event to a Xenta Schedule in WebStation
  • Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation
  • Editing or Deleting an Exception Event in a Xenta Schedule in WebStation
  • Assigning a Xenta Central Schedule in WebStation
  • Unassigning a Xenta Central Schedule in WebStation
  • Assigning a Lead Xenta Central Schedule in WebStation
  • Unassigning a Lead Xenta Central Schedule in WebStation