earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
规格

规格


产品: WebStation
功能: 警报, 基本功能, 图形, 时间表, 趋势
产品版本: 7.0
2025/7/4

WebStation

arrow1_rotation简介 arrow1_rotation特点 arrow1_rotation软件许可模式 arrow1_rotation规格
 
action_zoom_plus_stroke WebStation
图: WebStation

简介

EcoStruxure Building Operation WebStation 是一个基于 web 的用户界面,用于 EcoStruxure BMS 中的日常管理。WebStation 内置于每一个 EcoStruxure BMS 服务器中,允许用户从世界各地访问软件。

特点

WebStation provides a rich, responsive user interface to access the EcoStruxure BMS servers using common web browsers on Windows PCs, Mac OS computers, Android and iOS tablets and smartphones. Users can view and manage dashboards, slide shows, graphics, alarms, schedules, trend logs and user accounts.

Dashboards

The dashboard functionality enables users to create their own pages to get an overview of how buildings perform, using easy-to-use and easy-to-read data visualization components. Basic energy consumption monitoring, alarm statistics, and environmental summaries are presented in clear ways on any device.

 
action_zoom_plus_stroke 仪表板
图: 仪表板

The EcoStruxure BMS software has a set of built-in components for visualization of live and historical data, including interactive widgets for alarm and event statistics to help management of alarms. For customers with additional requirements, custom dashboard components can be developed using the powerful graphics capabilities.

Semantics

With the support for semantic modelling using Brick Schema, WorkStation and WebStation provide users with enhanced contextual information. Using Brick Schema, users can easily see where alarms originate from, what areas are affected and where to find root causes. The system can be navigated, searched, and filtered using understandable information about locations, equipment, point types and their relationships. WorkStation and WebStation also provide automatically generated alarm views, trend charts and schedule views for the modelled entities. For example, when selecting a floor in a building, the system automatically provides an alarm view filtered for alarms that originate from sources that are related to that floor.

 
action_zoom_plus_stroke 语义视图
图: 语义视图
Meter management

With the meter management functionality, EcoStruxure Building Operation offers improved methods to ensure data is accurate and meter changes are automatically detected. In addition, purpose-built functions enable easier handling of the following concepts:

  • Aggregations

  • Virtual metering

  • Apportioned metering

  • Unit conversions

Meter hierarchies enable powerful visualization of sub-meter structures or categorizations. A web-based editor with intelligent help functions enables efficient construction of meter hierarchies.

Normalization and signatures

The normalization functions help with benchmarking, and the signature function enables automation and/or alerting when resource usage is too high or low. This enables early detection of faulty equipment and misused building functions, resulting in energy savings and higher occupant satisfaction.

The system includes easy-to-use tools for regression analysis and powerful methods for time-period classification, that is, differentiation of workdays versus holidays.

Compliance for regulated industries

Using the built-in security features within the EcoStruxure BMS software, you can comply with 21 CFR Part 11 and other Life Sciences regulations, restricting access to authorized and qualified individuals and with full audit trail. In addition, the built-in access and security settings can be enhanced by applying further restrictions and limit access by time-of-day or geographic location.

The change control features extend the basic activity logging provided by the EcoStruxure BMS software by enhancing the functionality of the standard log, enabling efficient and fully configurable change control with the following features:

  • Single or dual electronic signature application

  • Change control that can be restricted only to specific objects in the system

  • Change control that can easily be applied to all objects

  • Every associated action is logged with the parameter that was changed

  • Before and after parameter values including meta data

For each signature event, the change control signatures contain:

  • The unique identifier of the person executing the signature

  • The full name of the user who performed the action

  • The geographical date and time stamp

  • The meaning of the signature, such as approval, review, responsibility, and authorship

Slide shows

For public displays, the slide show can automatically switch between dashboards to provide up-to-date information for building occupants.

Secure user accounts

An EcoStruxure BMS requires each user to have an account. Access can be through an account maintained by the EcoStruxure BMS database or through a Windows Active Directory account. IT policies for password formatting, aging, and uniqueness are supported and enforced. Access rights can be assigned based on schedule and/or client IP address.

软件定义的分区

WebStation 能够通过可选分区插件许可证实现非常容易地重新配置联网房间解决方案功能。图形或表格视图可实现从任何 Web 浏览器设备快速编辑 HVAC、百叶窗和照明如何在房间控制器范围内或各房间控制器之间实现同步。

 
action_zoom_plus_stroke 分区视图
图: 分区视图
Language and regional settings

The software adapts the displayed language, measurement system, and date/time format to the operating system settings. Language and measurement system can easily be switched from within WebStation. Translations of WebStation are delivered as separate language packs that are easy to install and deploy. More than 40 preset data and time formats are supported. Administrators can configure localization defaults to save end users from having to edit the regional settings.

Customized view of the system

The software has the flexibility to be fully customized to the viewing preference of each user. In the main interface, called the Workspace, users can select a wide variety of components, such as custom menus, alarms, graphics, and editors. WebStation supports Workspace and Panel functionality without modification and automatically adapts the layout to the device used.

Powerful search functionality

The search function helps users quickly find information and navigate to wherever they need to go. By typing in all or part of the name, the user sees a list of all items that match. The software shows the current status or value for each item and users can open the item directly from the search list.

Efficient alarm management

Alarms need to be assessed and responded to quickly. Through the user interface, alarms are displayed in a simple and efficient way to ensure that no alarm is overlooked. Alarms can be color coded, grouped, and filtered for maximum efficiency. The user interface enables dispatch centers or managers to assign alarms to a user or a group of users. Using a filter, users can see only the alarms assigned to them and accept or reject the assignment.

 
action_zoom_plus_stroke 警报视图
图: 警报视图

Filter settings and layout can be edited and stored as Favorites in the Alarms view and the Events view. Quick filter enables fast filtering of the views. Multiple alarms can be batch acknowledged for effective alarm management.

Robust alarm tracking

Alarms can be acknowledged with varying degrees of detail, depending on the importance of the alarm. Users can be required to enter notes or choose from a standard list to explain how the issue was resolved. WebStation can present the user with instructions or a specific view of their system that shows details of the affected equipment. The audit trail records the user’s actions.

Stunning graphics capability

In an EcoStruxure BMS, the graphics can be customized to provide the user interface required to effectively run each facility. Graphics are stored locally in the EcoStruxure BMS servers and are available to authorized users from wherever they log on.

Scalable vector graphics

The EcoStruxure BMS software uses scalable vector graphic technology so that users can zoom in to see details without losing clarity. Graphics are built once, but can be used on any display regardless of size or resolution. Vector graphic file sizes are small so they can be stored and served directly from the SpaceLogic automation server.

Super dynamic live updates

A standard live update simply shows the displayed values as conditions change in the field. With the EcoStruxure BMS software's super dynamic live updates, all aspects of graphical elements can change when values change.

Advanced activity log

It is important to log more than basic activity. The software logs every action with a timestamp, the user who performed the action, and the values that were changed.

Easy to read trend logs and charts

The software can trend data in many ways, including a periodic method (every day, hour, minute) and a change-of-value (COV) method that only records when a defined threshold has been passed. These trend logs can be shown in trend lists and charts to visualize patterns for diagnostic and optimization purposes. Multiple series can be presented in a single chart, so that data points can be easily compared.

 
action_zoom_plus_stroke  趋势图视图
图: 趋势图视图

The color, weight, and style of all lines can be specified. Display of digital data is automatically shown as high and low horizontal bars, eliminating the need for additional scaling. Log data can be presented as average, minimum, maximum, or delta in addition to the actual log value itself. Users can zoom in to see details without losing clarity. A trend chart can have two different scales on the same chart to see how different data relate to each other.

Trend data can be exported and downloaded as Excel files.

IT friendly and secure

WebStation is based on standard web technologies and requires no special configuration on the client or server side. Platform-independent technologies make it run on most popular browsers. No Schneider Electric specific software has to be installed and maintained on the client computers and no browser plug-ins are needed.

TLS support

Communication between clients and the EcoStruxure BMS servers can be encrypted using Transport Layer Security (TLS) . The servers are delivered with a default self-signed certificate. Commercial Certification Authority (CA) server certificates are supported to lower the risk of malicious information technology attacks. Use of encrypted communication can be enforced for both WorkStation and WebStation access.

Intuitive schedules

Energy efficiency is achieved when equipment is running only when necessary. Schedules manage that process through a graphical interface that is easy-to-use. Change times with a few simple clicks of the mouse. The powerful Schedule Editor can set up recurring events (every Monday, every third Tuesday, or every January 1st) or an unlimited number of exceptions with priority levels. Schedules go beyond the basic on and off control by enabling direct control of analog values. For example, users can set schedule events to percentages to control lighting levels without writing a program.

 
action_zoom_plus_stroke 时间表编辑器
图: 时间表编辑器

WebStation also provides a powerful combined view of multiple schedules, which allows simple editing of many schedules in a single operation.

 
action_zoom_plus_stroke 多时间表编辑器
图: 多时间表编辑器
Function Block program viewer

WebStation offers a built-in, quick and easy way to view the contents of Function Block programs, allowing users to get a more detailed view of the program logic, including a live view of inputs, outputs, and other values.

 
action_zoom_plus_stroke 功能块程序查看器
图: 功能块程序查看器

软件许可模式

EcoStruxure BMS software version 7.0 offers a simplified and centralized licensing model which allows for one-time, single-step activation of a system license deployed at the top level server of the system, thus removing the need for license engineering on each server in the system. This provides considerable time savings during the initial commissioning as well as during any future upgrade of the system.

System capabilities are available in a three-tier model: Essential, Advanced, and Advanced Plus. Select the tier that matches your business needs, and everything will then be bundled into the centralized system license and inherited across all servers in your system architecture, including Enterprise Central, Enterprise Server, and field servers.

The centralized licensing model combined with the three-tier capability model provides a uniquely easy-to-manage system throughout the lifecycle. Among other benefits, this gives the ability to remotely manage the capability tier as business needs evolve and to facilitate expansion as the system grows with added servers and connected devices.

Configuration of software licenses is done through EcoStruxure Power & Building Software Companion, accessible by EcoXpert™ partners and Schneider Electric representatives. It provides the ability to select architecture and tier options as well as manage license evolutions throughout the lifecycle of the system.

For more information on the three-tier system capabilities, see the Schneider Electric website, www.se.com .

规格

Server side
请参阅 SpaceLogic AS-P 服务器、SpaceLogic AS-B 服务器、边缘服务器、Enterprise server 和 Enterprise Central 规格表。 
Client-side hardware
Display
Minimum: 320x568 pixel resolution
  
Recommended: 1,024x768 pixel resolution, portrait and landscape mode
Other devices
A pointing device such as a mouse or touchscreen.
Client-side software
Web browser support
Minimum web browser versions required
Google Chrome 119 and later
  
Mozilla Firefox 119 and later
  
Microsoft Edge 119 and later
  
Safari 14 and later
Recommended web browser versions
Google Chrome latest
  
Mozilla Firefox latest
  
Microsoft Edge latest
  
Safari latest
Communication (to EcoStruxure BMS servers)
HTTP
Non-binary, port configurable, default 80
HTTPS
Encrypted supporting TLS 1.3, port configurable, default 443
 
action_zoom_plus_stroke WebStation 界面示例
图: WebStation 界面示例
 
action_zoom_plus_stroke WebStation 界面示例
图: WebStation 界面示例
 
action_zoom_plus_stroke WebStation 界面示例
图: WebStation 界面示例
 
action_zoom_plus_stroke WebStation 界面示例
图: WebStation 界面示例
  • Building Operation WebStation Overview
  • SpaceLogic AS-P
  • SpaceLogic AS-B
  • Enterprise Server
  • Enterprise Central
  • 边缘服务器