You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. For more information, see Licenses .
Select a Server hypertext transfer protocol option for communciation with the EcoStruxure BMS server.
In the Server box, enter an EcoStruxure BMS server name or an IP address.
You can also, in the scroll down menu, choose a server host name from the list. When you start typing the host name or the IP number of the server, you will be offered suggestions from the saved list.
When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.
Select Log on as to log on under the Windows user account you used to log on to the computer.
Select Remember me on this computer to have WorkStation remember your settings.
Click Log on .
You can register the system now or later:
Click Register now to register your system. For more information, see System Registration .
Click Register later to skip registration and register at a later time.