earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendências
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Create Trend Log Wizard – Initial Meter Settings Page

Use the Initial Meter Settings page to set the initial values for the meter.

 
action_zoom_plus_stroke Initial Meter Settings page
Imagem: Initial Meter Settings page

Tabela: Initital Meter Settings Page

Property

Description

Set initial meter

Select True to enable the meter function.

Start time

Enter the time when the new meter was installed.

Start value

Enter the value of the new meter when it was installed.

Min value

Enter the first value of the new meter after roll-over.

Max value

Enter the last value of the new meter before roll-over.

  • Meter Function
  • Trend Log Types