earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/3

Create Trend Log Wizard – Initial Meter Settings Page

Use the Initial Meter Settings page to set the initial values for the meter.

 
action_zoom_plus_stroke Initial Meter Settings page
图: Initial Meter Settings page

表格: Initital Meter Settings Page

Property

Description

Set initial meter

Select True to enable the meter function.

Start time

Enter the time when the new meter was installed.

Start value

Enter the value of the new meter when it was installed.

Min value

Enter the first value of the new meter after roll-over.

Max value

Enter the last value of the new meter before roll-over.

  • Meter Function
  • Trend Log Types