earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2.0, 2.1, 3.0, 3.1
10/30/2018

Unit Conversion Exceptions View

Use the Unit Conversion Exceptions view to override regional settings within a domain.

 
action_zoom_plus_stroke Unit Conversion Exceptions view
Figure: Unit Conversion Exceptions view

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a unit conversion exception to the list.

 
action_zoom_plus_stroke

Remove

Click to remove a unit conversion exception from the list.

 
action_zoom_plus_stroke

Show/Hide Group Box

Click to display the Show/Hide Group box to group and sort objects. For more information, see Group and Sort Objects .

Quick filter

Enter a word or a character to filter on. For more information, see Quick Filter .

Configured Unit

Enter the configured unit that is to trigger a conversion exception. The configured unit is the unit that is native to the value/object before being localized by any operating system.

SI Display Unit

Enter how the configured unit is to be displayed in an SI metric system.

US Display Unit

Enter how the configured unit is to be displayed in a US customary system.

Note:

Users in a domain become subjects to added unit conversion exceptions the next time they log on.

  • Units