The EcoStruxure Building Operation software supports both the SI metric system and the US Customary System for units of measurement.
There are four optional ways to display units:
For example, the temperature 42,82 °C is stored in the EcoStruxure Building Operation software. A WorkStation on an operating system with the US Customary System converts the temperature and displays it as 109.08 °F.
As MS Windows
By default, values are converted into the unit given by the regional settings of the operating system.
As configured in object
Units displayed as configured in the object means that no conversion is done. The unit the user selected when creating, for example, a trend log is displayed regardless of regional settings. When this option is selected, the unit conversion exceptions feature is disabled.
International System of Units (Metric)
Values displayed in International System of Units means that the values are converted into metric unit regardless of the unit the object was given when created.
United States Customary Units (US)
Values displayed in United States Customary Units means that the values are converted into US unit regardless of the unit the object was given when created.
When you select a different unit system, the values are converted immediately.
Values are not converted in the following WorkStation screens:
Delta Temperature Conversion
The conversion between Celsius and Fahrenheit or Fahrenheit and Kelvin is not a simple coefficient (multiplier) like other unit categories as for example length, pressure, currency, and Energy. Due to the conversion formula when for example converting an absolute Fahrenheit temperature to Celsius, T°F=T°C x 9/5 + 32, you have both a multiplier and an offset to consider. To correctly convert a delta temperature from Fahrenheit to Celsius you have to use the formula ΔT°F = 9/5 ΔT°C.
有关更多信息,请参阅 Delta Temperature Conversion
.