earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2024, 7.0
2024/12/3

Adding a Unit Conversion Exception

You add unit conversion exceptions to override the selected unit conversion system. If you have selected to display units as configured in object, the unit conversion exceptions feature is disabled.

显示更多
action_close

The EcoStruxure Building Operation software supports both the SI metric system and the US Customary System for units of measurement.

There are four optional ways to display units:

  • As MS Windows

  • As configured in object

  • International System of Units (Metric)

  • United States Customary Units (US)

For example, the temperature 42,82 °C is stored in the EcoStruxure Building Operation software. A WorkStation on an operating system with the US Customary System converts the temperature and displays it as 109.08 °F.

As MS Windows

By default, values are converted into the unit given by the regional settings of the operating system.

As configured in object

Units displayed as configured in the object means that no conversion is done. The unit the user selected when creating, for example, a trend log is displayed regardless of regional settings. When this option is selected, the unit conversion exceptions feature is disabled.

International System of Units (Metric)

Values displayed in International System of Units means that the values are converted into metric unit regardless of the unit the object was given when created.

United States Customary Units (US)

Values displayed in United States Customary Units means that the values are converted into US unit regardless of the unit the object was given when created.

When you select a different unit system, the values are converted immediately.

Values are not converted in the following WorkStation screens:

  • Alarms and trend logs in wizards

  • Customized alarm views

  • Alarm and trend log properties panes

Delta Temperature Conversion

重要:
  • The EcoStruxure Building Operation software converts the unit of a variable independent of its context. To correctly convert a delta temperature, the unit of the delta value must belong to the unit category Temperature Diff.

The conversion between ​Celsius and Fahrenheit or ​Fahrenheit and Kelvin is not a simple ​coefficient (multiplier) like other unit categories as for example length, pressure, currency, and Energy. Due to the conversion formula when for example converting an absolute ​Fahrenheit temperature to Celsius​, T​°F=T​°C x 9/5 + 32, ​ you have both a multiplier and an offset to consider. To correctly convert a delta temperature from ​​Fahrenheit to ​Celsius​ you have to use the formula ΔT°F = 9/5 ΔT°C.

有关更多信息,请参阅 Delta Temperature Conversion .

To add a unit conversion exception
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Domains .

  4. In the Domains list, select a domain for the unit conversion exception.

  5. Click Unit Conversion Exceptions .

  6. In the Unit Conversion Exceptions view, click Add

     
    action_zoom_plus_stroke
    .

  7. In the Unit Selection dialog box, select the unit for which you want a conversion exception.

  8. Click Select .

  9. In the Unit Conversion Exceptions view, in the SI Display Unit column, select the unit to be displayed in an SI metric system.

  10. In the US Display Unit column, select the unit to be displayed in a US customary system.

  11. Click the Save button

     
    action_zoom_plus_stroke
    .

The unit conversion exception takes effect immediately unless unit conversion is disabled.

  • Units
  • Control Panel Tab
  • Unit Conversion Exceptions View
  • Select Unit Dialog Box
  • Removing a Unit Conversion Exception