earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023
2022-03-17

WebStation in Kiosk Mode

arrow1_rotationKiosk Mode arrow1_rotationRemove the Toolbars from WebStation

You can configure to run WebStation in kiosk mode when you want to limit the users’ access to a web browser.

Kiosk Mode

You can display WebStation in kiosk mode with web browsers that supports kiosk mode. Refer to the browser documentation on how to use kiosk mode.

When kiosk mode is used, the toolbar, menus, and right-click menu, are disabled in the web browser. Most keyboard shortcuts, such as alt + F4 to close Internet Explorer, still work.

Use the guest log on if you want the user to get immediate access to WebStation in kiosk mode.

Remove the Toolbars from WebStation

You can remove the toolbars from WebStation in both kiosk mode and without kiosk mode.

Use the syntax /?kiosk=1#/ to remove all toolbars.

The text string /?kiosk=1#/ must be placed after the server address.

For example, you want to run this automation server without any toolbars:

https://10.142.0.227/#%2FAutomation%20Server

You add the /?kiosk=1#/

https://10.142.0.227/?kiosk=1#/Automation%20Server

Uwaga

The /?kiosk=1#/ does not configure the browser to run in kiosk mode. It only removes the toolbars.

  • Workspace Management