earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos Enterprise Central, Enterprise Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022, 2023
01/09/2020

Archive Settings Manager Dialog Box

Use the Archive Settings Manager to archive events, trend logs, and extended trend logs on the Enterprise Server or Enterprise Central.

 
action_zoom_plus_stroke Archive Settings Manager dialog box
Figura: Archive Settings Manager dialog box

Tabla: Archive Settings Manager Dialog Box

Number

Description

Enabled

Select to activate the archiving function on the Enterprise Server or Enterprise Central. Para obtener más información, consulte Enabling the Archiving Function and Defining the Archive Folder .

Disabled

Select to disable the archiving function on the Enterprise Server or Enterprise Central.

Update Archive Now

Click to archive the selected historical data immediately. Para obtener más información, consulte Manually Creating an Archive .

Alarm Events

Select to include Alarm events in the archive.

User Events

Select to include User events in the archive.

System Events

Select to include System events in the archive.

 
action_zoom_plus_stroke

Click to add an extended trend log to the list.

 
action_zoom_plus_stroke

Click to delete an extended trend log from the list.

Extended Trend Log

Select the logs that you want to include in the archive.

Archive Schedule

Click Schedule to configure a schedule for archiving. Para obtener más información, consulte Manual and Scheduled Archiving .

Output Type

Select an output type for the archive. Para obtener más información, consulte Archive Formats and Storage .

Path

Type the path to the location where you want store the archive files. Para obtener más información, consulte Enabling the Archiving Function and Defining the Archive Folder .

Validate

Click to validate that the path is valid. A green checkmark

 
action_zoom_plus_stroke
displays if the system successfully validates the path.

  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • Manually Creating an Archive
  • Manual and Scheduled Archiving
  • Archive Formats and Storage