earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/3

Archive Settings Manager Dialog Box

Use the Archive Settings Manager to archive events, trend logs, and extended trend logs on the Enterprise Server or Enterprise Central.

 
action_zoom_plus_stroke Archive Settings Manager dialog box
图: Archive Settings Manager dialog box

表格: Archive Settings Manager Dialog Box

Number

Description

Enabled

Select to activate the archiving function on the Enterprise Server or Enterprise Central. 有关更多信息,请参阅 Enabling the Archiving Function and Defining the Archive Folder .

Disabled

Select to disable the archiving function on the Enterprise Server or Enterprise Central.

Update Archive Now

Click to archive the selected historical data immediately. 有关更多信息,请参阅 Manually Creating an Archive .

Alarm Events

Select to include Alarm events in the archive.

User Events

Select to include User events in the archive.

System Events

Select to include System events in the archive.

 
action_zoom_plus_stroke

Click to add an extended trend log to the list.

 
action_zoom_plus_stroke

Click to delete an extended trend log from the list.

Extended Trend Log

Select the logs that you want to include in the archive.

Archive Schedule

Click Schedule to configure a schedule for archiving. 有关更多信息,请参阅 Manual and Scheduled Archiving .

Output Type

Select an output type for the archive. 有关更多信息,请参阅 Archive Formats and Storage .

Path

Type the path to the location where you want store the archive files. 有关更多信息,请参阅 Enabling the Archiving Function and Defining the Archive Folder .

Validate

Click to validate that the path is valid. A green checkmark

 
action_zoom_plus_stroke
displays if the system successfully validates the path.

  • Enabling the Archiving Function and Defining the Archive Folder
  • Creating a Scheduled Archive
  • Manually Creating an Archive
  • Manual and Scheduled Archiving
  • Archive Formats and Storage