earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
10/24/2018

Actions Menu – Actions Submenu

Use the Actions submenu to create manual archives from an Enterprise Server or an Enterprise Central.

 
action_zoom_plus_stroke Actions Menu – Actions submenu
Figure: Actions Menu – Actions submenu

Table: Actions Menu – Actions Submenu

Command

Description

Create archive(s) now

Creates a manual archive that is saved to a predefined path on the computer running WorkStation. For more information, see Archive Settings Manager Dialog Box .

  • Manual and Scheduled Archiving
  • Archive Settings Manager Dialog Box
  • Manually Creating an Archive