earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : Enterprise Server, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
23/10/2018

Add Extended Trend Logs Dialog Box

Use the Add Extended Trend Logs dialog box to include logs in an archive. The system only lists the logs on the Enterprise Server or Enterprise Central that are not included the archive.

 
action_zoom_plus_stroke Add Extended Trend Logs dialog box
Figure : Add Extended Trend Logs dialog box

Table : Add Extended Trend Logs Dialog Box

Component

Description

 
action_zoom_plus_stroke

Click to include all the listed extended trend logs in the archive operation.

 
action_zoom_plus_stroke

Click to exclude all the extended trend logs selected for the archive operation.

Include

Select the extended trend logs that you want to include in the archive.

Extended Trend Log

Displays the name and the location of the extended trend log on the Enterprise Server or Enterprise Central.

  • Manually Creating an Archive
  • Creating a Scheduled Archive