Produkty: Enterprise Server, Project Configuration Tool
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-10-23

Add Extended Trend Logs Dialog Box

Use the Add Extended Trend Logs dialog box to include logs in an archive. The system only lists the logs on the Enterprise Server or Enterprise Central that are not included the archive.

 
action_zoom_plus_stroke Add Extended Trend Logs dialog box
Rysunek: Add Extended Trend Logs dialog box

Tabela: Add Extended Trend Logs Dialog Box

Component

Description

 
action_zoom_plus_stroke

Click to include all the listed extended trend logs in the archive operation.

 
action_zoom_plus_stroke

Click to exclude all the extended trend logs selected for the archive operation.

Include

Select the extended trend logs that you want to include in the archive.

Extended Trend Log

Displays the name and the location of the extended trend log on the Enterprise Server or Enterprise Central.

  • Manually Creating an Archive
  • Creating a Scheduled Archive