earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/10/23

Add Extended Trend Logs Dialog Box

Use the Add Extended Trend Logs dialog box to include logs in an archive. The system only lists the logs on the Enterprise Server or Enterprise Central that are not included the archive.

 
action_zoom_plus_stroke Add Extended Trend Logs dialog box
图: Add Extended Trend Logs dialog box

表格: Add Extended Trend Logs Dialog Box

Component

Description

 
action_zoom_plus_stroke

Click to include all the listed extended trend logs in the archive operation.

 
action_zoom_plus_stroke

Click to exclude all the extended trend logs selected for the archive operation.

Include

Select the extended trend logs that you want to include in the archive.

Extended Trend Log

Displays the name and the location of the extended trend log on the Enterprise Server or Enterprise Central.

  • Manually Creating an Archive
  • Creating a Scheduled Archive