Productos WorkStation
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
16/11/2018

Cómo guardar detalles de inicio de sesión

Para iniciar sesión más rápidamente, use la función Recordarme y completar así automáticamente sus datos.

Aviso
  • Por razones de seguridad, su contraseña no se rellena automáticamente.

Mostrar más
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.

Aviso

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Para obtener más información, consulte EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

Para guardar sus datos de inicio de sesión
  1. En la ventana de Bienvenida, seleccione Recuérdame (en este equipo) .

  2. Haga clic en Inicio de sesión .

  • Log on to WorkStation or WebStation
  • Inicio de sesión en WorkStation como usuario de EcoStruxure Building Operation
  • Inicio de sesión en WorkStation como otro usuario de Windows
  • Selección de un entorno de trabajo predeterminado
  • Cambio entre los entornos de trabajo
  • Cierre de sesión en WorkStation
  • Cómo salir de WorkStation
  • Changing Your Password
  • Building Operation WorkStation Window