earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Energy Unit Configuration Errors

When you run one of the three different types of energy reports, it is possible that the report contains an error message informing you that energy units are not configured correctly. For example, you configured a power unit (W) instead of an energy unit (Wh), or you did not assign any unit at all. In these circumstances you need to know which extended trend log is incorrectly configured, and you can find out by clicking directly on the error message link. The subsequent report contains details of relevant trend logs and of the associated energy meter.

For example, you run a Consumption report on Electricity Meter 1 and you see the Units are not configured correctly message:

 
action_zoom_plus_stroke Units are not configured correctly message
Figure: Units are not configured correctly message

If you click on the error message link, a Unit Configuration Errors report is generated (in this example, units have not been configured):

 
action_zoom_plus_stroke Location of extended trend log configuration error
Figure: Location of extended trend log configuration error

You can also generate a Unit Configuration Errors report from the WebReports Diagnostics folder. For more information, see Unit Configuration Errors Report .

You can configure the extended trend log to correct the energy units error. For more information, see Configuring an Extended Trend Log .

  • Configuring an Extended Trend Log
  • Unit Configuration Errors Report
  • WebReports Diagnostic Reports
  • Energy Monitoring Reports