When you run one of the three different types of energy reports, it is possible that the report contains an error message informing you that energy units are not configured correctly. For example, you configured a power unit (W) instead of an energy unit (Wh), or you did not assign any unit at all. In these circumstances you need to know which extended trend log is incorrectly configured, and you can find out by clicking directly on the error message link. The subsequent report contains details of relevant trend logs and of the associated energy meter.
For example, you run a Consumption report on Electricity Meter 1 and you see the Units are not configured correctly message:
If you click on the error message link, a Unit Configuration Errors report is generated (in this example, units have not been configured):
You can also generate a Unit Configuration Errors report from the WebReports Diagnostics folder. Pour plus d'informations, voir Unit Configuration Errors Report .
You can configure the extended trend log to correct the energy units error. Pour plus d'informations, voir Configuration d'un journal de tendance étendu .