earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 用户管理
产品版本: 2024, 7.0
2024/12/2

Workspace Customization

You customize the workspace layout to control access and meet the specific requirements of a user account group. For example, you hide or show panes and toolbars. You can save a workspace layout on the EcoStruxure BMS server. In this case, the layout becomes the default workspace layout for all users in the user account group the workspace belongs to. Workspaces are task oriented, which means that a user can switch workspaces during a single WorkStation session.

You can configure a workspace to contain a limited number of views to which users have access. Specifically, you can add, edit, move, or remove the following panes and windows:

  • Advanced Schedule Pane

  • Alarms Pane

  • Basic Schedule Pane

  • Calendar Pane

  • Events Pane

  • Function Block Program Pane

  • Graphic Pane

  • Multi Trend Log List Pane

  • Navigation Pane

  • Panel Pane

  • System Tree Pane

  • Trend Chart Pane

  • Trend Log List Pane

  • Watch Pane

  • Work Area Window

For example, you can create a workspace that displays an Alarms pane and a graphic in the work area representing a building.

Customized Navigation

You use the Navigation Pane to build a customized structure for navigation. The Navigation pane can be used in a workspace or a panel.

有关更多信息,请参阅 Customized Navigation .

Workspace Path, Object, and Command Customization

Software permissions limit the paths, objects, and commands that are available in a workspace. For example, a user with No Access permissions for a particular path cannot see any of the path objects displayed in the System Tree pane. A user with Read permissions for a path can see the path objects but cannot issue any commands because the objects are not made available.

有关更多信息,请参阅 Workspace Path, Object, and Command Customization .

  • Workspace Components and Customization
  • Resetting the Workspace Layout
  • Resetting All User Settings
  • Customized Navigation
  • Workspace Path, Object, and Command Customization