earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
12/11/2018

Action Note Group Properties

Use the Action Note Group Properties view or dialog box to view or edit the properties of the Action Note Group.

 
action_zoom_plus_stroke Action Note Group properties
Figure: Action Note Group properties

Table: Action Note Group Properties

Property

Description

Name

Displays the name of the action notes in the action note group. For more information, see Action Notes .

 
action_zoom_plus_stroke

Add

Click to open the Action Note wizard.

 
action_zoom_plus_stroke

Edit

Click to open the properties dialog box for the selected action note. For more information, see Action Note Properties .

 
action_zoom_plus_stroke

Remove

Click to remove the selected action note.

  • General Information Properties – Basic Tab
  • Action Notes
  • Action Note Properties