earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
12/11/2018

Action Note Properties

Use the Action Note Properties view or dialog box to type the display name of the action note and to configure and view the general and object reference properties. For more information, see General Information Properties – Basic Tab .

 
action_zoom_plus_stroke Action Note properties
Figure: Action Note properties

Table: Action Note Properties

Property

Description

Action note

Type the display name of the action note. For more information, see Action Notes .

  • General Information Properties – Basic Tab
  • Action Notes
  • Action Note Group Properties