earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2023
2022/12/17

Setting the Automatic Logoff Time

Use the automatic logoff function to avoid access by unauthorized users and ensure that WorkStation users do not occupy a license they are not using.

显示更多
action_close

The automatic logoff function makes it possible for the system to automatically log off a user after a specified time of inactivity.

Inactivity means that no user-initiated activity using the mouse or keyboard has been made. However, if a user has has started a large task in Workstation, for example an import or a large copy and paste, the user is still considered to be active as long as the process is ongoing in Workstation.

The automatic logoff function increases security and ensures that WorkStation users do not occupy licenses they are not using.

When a user is logged off by the automatic logoff function all settings that are not saved are lost.

The automatic logoff time is set at user group level. If a user belongs to more than one group, the automatic logoff time for the user is defined by the group that has the longest automatic logoff time.

For example, a user belongs to two groups: a group with the automatic logoff time of five minutes and a group with the automatic log off time of 15 minutes. The automatic logoff time for the user is 15 minutes.

If a user is belongs to a group that does not have the automatic log off function enabled, the user is never logged off.

The default local admin account is logged off after ten minutes of inactivity. You cannot change this setting.

To set the automatic logoff time
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the Server list, select the EcoStruxure BMS server containing the user account group you want to set the auto log off time for.

  5. In the Domain list, select the domain the user account group belongs to.

  6. In the User Account Groups list, select the user account group.

  7. Click Policies .

  8. Select Automatic logoff and then select the number of minutes a user in the user account group can be idle before being logged off.

  • Automatic Logoff
  • Control Panel Tab