earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Central, Enterprise Server, Software Administrator
功能: 工程
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/5/18

Software Administrator

arrow1_rotationService arrow1_rotationPorts arrow1_rotationDatabase Location arrow1_rotationEnterprise Server and Enterprise Central System Logs

The Software Administrator installs with the Enterprise Server and Enterprise Central installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server and Enterprise Central.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.

Service

The Enterprise Server and Enterprise Central run in the background as Windows services. You start and stop the server services through the Software Administrator or Windows Service. Before shutting down a server, make sure the stop does not negatively affect your site.

Ports

The Enterprise Server and Enterprise Central use HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server or Enterprise Central service.

注释:

Port changes you have made using Software Administrator are not automatically updated in the Communication view for EcoStruxure BMS servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server or Enterprise Central write and store data and objects that are created by either the Enterprise Server, Enterprise Central, or the user.

Enterprise Server and Enterprise Central System Logs

The Enterprise Server and Enterprise Central System logs contain events logged by the Enterprise Server or Enterprise Central. Examples of logged events are startup sequence, port settings, failures, run time, and current server status.

  • Starting the Enterprise Server or Enterprise Central Windows Service
  • Stopping the Enterprise Server Windows Service
  • Restarting the Enterprise Server Windows Service
  • Starting the Enterprise Central Windows Service
  • Stopping the Enterprise Central Windows Service
  • Software Administrator – Enterprise Server View
  • Software Administrator – Enterprise Central View
  • ​Configuring Server Port Settings
  • Products
  • Installation Overview
  • EcoStruxure BMS Server Management
  • Resolving Enterprise Server or Enterprise Central Port Conflicts