earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Basic Functionality, Trends
Product version: 2024, 7.0
12/3/2024

Add/Remove Columns Dialog Box (Trends)

Use the Add/Remove Columns dialog box to add or remove columns from the trend log list.

 
action_zoom_plus_stroke Add/Remove Columns dialog box
Figure: Add/Remove Columns dialog box

Table: Add/Remove Columns Dialog Box

Component

Descriptin

Comment

Select to display the comment added by a user or system. For more information, see Comments .

Events

Select to display any events that occurred.

Sample status

Select to display the condition when the sample was recorded.

Sequence number

Select to display the event sequence number on the present EcoStruxure BMS server.

Time stamp

Select to display the time and date when the event was generated.

User

Select to display the user name that generated the event.

Value

Select to display the value.

  • Trend Log Lists
  • Add/Remove Columns Dialog Box
  • Quick Filter