earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9
2013/6/17

Editing a Factory Supplied Report

You edit a factory supplied report to customize it to your requirements.

显示更多
action_close

Report Builder is a separately downloadable part of Microsoft SQL Server 2008 and SQL Server 2012, and provides the facility for you to create, modify, and deploy your own reports to the Reports Server, based on selected parts of the Building Operation database.

Using Report Builder, you can use wizards to create a table, map, chart, or matrix as the basis for your report. The data content of your report is based on the selection of datasets within the Building Operation data source (StruxureWareReportsDB) in SQL Server 2008 or SQL Server 2012.

You can also modify existing factory supplied reports that are provided with the WebReports installation.

When you have built and formatted a report, you can deploy it to the Reports Server. You then synchronize the report with WebReports so that the report is displayed in the Reports Tree in a web browser.

After the reports is synchronized with WebReports, you cannot rename or delete the reports. Even if you delete reports from Report Manager, the reports will still be displayed in Reports Tree of WebReports.

注释:

The Report Builder section of this reference guide provides basic report customization procedures, and every effort is made to ensure that the information provided is accurate. For more detailed information about the Report Builder third-party software, please refer to the Microsoft Report Builder Online Help.

To edit a factory supplied report
  1. In MS Report Builder, click the main menu button, and then click the Options button.

     
    action_zoom_plus_stroke
  2. In the Use this report server box , type http://localhost/reportserver_SQLEXPRESS .

     
    action_zoom_plus_stroke
  3. Click OK .

  4. Click the main menu button, and then click Open .

     
    action_zoom_plus_stroke
  5. Select the folder that contains the factory supplied report that you want to edit.

     
    action_zoom_plus_stroke
  6. Select your factory supplied report.

     
    action_zoom_plus_stroke
  7. Click Open .

     
    action_zoom_plus_stroke
  8. Right click the area of the report that you want to edit, and then select the properties command.

     
    action_zoom_plus_stroke
  9. Edit the properties as required.

     
    action_zoom_plus_stroke
  10. Click OK .

     
    action_zoom_plus_stroke
  11. Save your edited report to the required location.

     
    action_zoom_plus_stroke

You can now synchronize your edited report with WebReports. 有关更多信息,请参阅 Synchronizing WebReports with a New Report .

  • Reports in Report Builder
  • Synchronizing WebReports with a New Report