earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms, Basic Functionality, Schedules, Trends, User Management
Product version: 1.9
12/14/2016

Function Overview

arrow1_rotationAlarm Overview arrow1_rotationSchedules Overview arrow1_rotationTrend Overview arrow1_rotationUser Account Management Overview arrow1_rotationBackup and Restore Overview arrow1_rotationDocuments Overview arrow1_rotationSearch Overview arrow1_rotationShortcuts Overview

Building Operation gives you a number of functions to monitor and manage your facilities.

Alarm Overview

You use an alarm to monitor a variable and to alert you if the monitored variable matches the configured alarm conditions.

For more information, see Alarms Overview .

Schedules Overview

A schedule is a sequence of events that determines when essential events occur in a building automation system: doors locking or unlocking, temperature raised or lowered, or equipment turned on or off.

For more information, see Schedules Overview .

Trend Overview

The function of a trend log is to log the variable that it is connected to and store the records.

For more information, see Trends Overview .

User Account Management Overview

When logging on to a SmartStruxure server, you have to authenticate yourself by using a valid user account. The user account has to belong to the same domain as the server you log on to.

For more information, see User Account Management Overview .

Backup and Restore Overview

Backup and Restore assures that SmartStruxure server data can be restored after damage or loss due to hardware or software failures, security threats, or application testing.

For more information, see Backup and Restore Overview .

Documents Overview

A Document is a container in which you can upload (import) a file for use in Building Operation. You can upload all types of files, including reports, forms, images, and video clips.

For more information, see Documents Overview .

Search Overview

Use Search in WorkStation to find and view objects in the database.

For more information, see Search Overview .

Shortcuts Overview

In Building Operation, you can create shortcuts to objects in the System Tree pane. A shortcut is a link to a target SmartStruxure server, folder, or other object and is simply a pointer to an object which acts as if it is that object.

For more information, see Shortcuts Overview .

  • Building Operation Overview
  • Alarms Overview
  • Schedules Overview
  • Trends Overview
  • User Account Management Overview
  • Backup and Restore Overview
  • Documents Overview
  • Search Overview
  • Shortcuts Overview