earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, AS-P, Project Configuration Tool, WebReports, Script Editor, SmartX HMI Kiosk, SmartXKiosk
Funcionalidades: Programación, Ingeniería, Gráficos, Importar/Exportar, Informes
Versión del producto: 2.0, 2.1, 3.0, 3.1
15/10/2019

Engineering Tools Overview

You engineer your system using the engineering tools.

Spreadsheet Overview

You use the Spreadsheet view to create and edit multiple objects and to save time.

Para obtener más información, consulte Spreadsheet Overview .

Bindings Overview

A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The source supplies the value to the destination.

Para obtener más información, consulte Bindings Overview .

Text Reports Overview

A text report provides a simple and quick method of obtaining a customized view of object property attributes.

Para obtener más información, consulte Text Reports Overview .

Import and Export Overview

A solution or application is a user-created object or group of objects that perform a control process. Examples of creatable objects include networks, devices, programs, binding templates, graphics, trends, and alarms.

Para obtener más información, consulte Import and Export Overview .

Script Overview

Script programs are text-based instructions that tell the EcoStruxure BMS server to take some kind of action to control a building.

Para obtener más información, consulte Script Overview .

Function Block Editor Overview

Function Block Editor is a graphical programming tool for EcoStruxure BMS servers and MP Series controllers, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.

Para obtener más información, consulte Function Block Editor Overview .

Graphics Editor Overview

​You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.

Para obtener más información, consulte Graphics Editor .

WebReports Overview

​WebReports is a Web application that you use to create, view, and administer reports. The reports provide information about alarms, trends, and user and system activity. You use the reports to help manage your building automation system.

Para obtener más información, consulte WebReports Overview .

Project Configuration Tool Overview

Project Configuration Tool, with Project Configuration Tool client and WorkStation, is an offline engineering platform that is used for project configuration, virtual EcoStruxure BMS server configuration, and deployment. Project Configuration Tool supports the major communication protocols in the same way as other EcoStruxure Building Operation software products.

Para obtener más información, consulte Project Configuration Tool Overview .

Vista Conversion Overview

To assess whether or not to convert a Vista system to an EcoStruxure BMS, you run an analysis of the Vista database export file to get information on the potential outcome of a conversion. The analysis is performed in TAC Vista Conversion Tool. If the analysis confirms that the Vista database is suitable for conversion, you can convert the database in TAC Vista Conversion Tool.

Para obtener más información, consulte Vista Conversion Overview .

Continuum Conversion Overview

Conversion is the process by which a customer's site is moved from Andover Continuum's legacy Building Management System to the EcoStruxure BMS. The Continuum Conversion Tool takes an ASCII dump from the Continuum system and creates EcoStruxure Building Operation objects that correspond to the objects in the ASCII dump file.

Para obtener más información, consulte Continuum Conversion Overview .

SmartX HMI Kiosk Overview

SmartX HMI Kiosk allows you to configure AD v3 as a dedicated HMI for local access to EcoStruxure BMS servers.

Para obtener más información, consulte SmartX HMI Kiosk Overview .

SmartXKiosk Overview

SmartXKiosk allows you to configure AD v2 and AD v1 as a dedicated HMI for local access to EcoStruxure BMS servers.

Para obtener más información, consulte SmartXKiosk Overview .

SmartX AD-Link Overview

SmartX AD-Link allows you to use a USB connection for TCP/IP network communication between AD v2 or AD v1 and an EcoStruxure BMS server.

Para obtener más información, consulte SmartX AD-Link Overview .

  • EcoStruxure Building Management Overview
  • Spreadsheet Overview
  • Bindings Overview
  • Text Reports Overview
  • Import and Export Overview
  • Script Overview
  • Function Block Editor Overview
  • Graphics Editor
  • WebReports Overview
  • Vista Conversion Overview
  • Continuum Conversion Overview
  • SmartX HMI Kiosk Overview
  • SmartXKiosk Overview
  • SmartX AD-Link Overview