earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: AS-C, AS-B, Device Administrator, Enterprise Server, Function Block Editor, Graphics Editor, License Administrator, License Server, AS-P, Script Editor, Software Administrator
Funktionen: Basisfunktionalität, Lizenzverwaltung, Lokalisierung
Produktversion: 1.8, 1.9
10.06.2016

Licensing, Installation, and Localization Overview

To be able to run Building Operations you need to install and licensing the software.

Licensing Overview

Building Operation is available for all to download and install. However, you need valid licenses to use Building Operation. The number of users of the software is limited to the number of licenses owned by the customer.

Für weitere Informationen siehe Licensing Overview .

Installation Overview

The Building Operation products are installed using installation packages.

Für weitere Informationen siehe Installation Overview .

Regional and Language Overview

WorkStation presents language, date, time, currency, unit, and decimals according to the user’s operating system settings.

Für weitere Informationen siehe Regional and Language Overview .

  • Building Operation Overview
  • Licensing Overview
  • Installation Overview
  • Regional and Language Overview