To be able to run Building Operations you need to install and licensing the software.
Building Operation is available for all to download and install. However, you need valid licenses to use Building Operation. The number of users of the software is limited to the number of licenses owned by the customer.
For more information, see Licensing Overview .
The Building Operation products are installed using installation packages.
For more information, see Installation Overview .
WorkStation presents language, date, time, currency, unit, and decimals according to the user’s operating system settings.
For more information, see Regional and Language Overview .