To run the EcoStruxure Building Operation software, you need to install and license the software. To keep your system maintained and up to date, you need to upgrade the software.
The EcoStruxure Building Operation software products are installed using installation packages.
For more information, see Installation Overview .
A system upgrade can include an Enterprise Server, one or more field servers and WorkStations, and the supporting administrator software, such as Device Administrator.
For more information, see Upgrade Overview .
The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.
For more information, see Licensing Overview .