To be able to run the EcoStruxure Building Operation software you need to install and licensing the software.
The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.
Więcej informacji zawiera Licensing Overview .
The EcoStruxure Building Operation software products are installed using installation packages.
Więcej informacji zawiera Installation Overview .
WorkStation presents language, date, time, currency, unit, and decimals according to the user’s operating system settings.
Więcej informacji zawiera Regional and Language Overview .