earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Функции: Базовые функции, Разработка
Версия продукта: 7.0, 7.1
30.10.2025

Add/Remove Columns Dialog Box (Search)

Use the Add/Remove Columns dialog box to add or remove columns to the Search View.

Примечание

The columns that are displayed in the list are the columns that are relevant for the specific search result.

 
action_zoom_plus_stroke Add/Remove Columns dialog box default columns
Рисунок: Add/Remove Columns dialog box default columns

Таблица: Add/Remove Columns Dialog Box Default Columns

Component

Description

Description

Select to display what the object or property is used for.

Foreign address

Select to display the address to a non-EcoStruxure Building Management product, for example a BACnet device.

Modified

Select to display the date and time when the object was last modified.

Name

Select to display the name of the object or property.

Note 1

Select to display a text that appears in a graphic or search result.​

Note 2

Select to display a text that appears in a graphic or search result.

Path

Select to display the path of the object.

Property binding

Select to display the in-bound binding of the object property.

Property retain level

Select to display the retain level of the object property.

Type

Select to display the object type that defines the properties of the object

Validation

Select to display the value of the validation property of the object.

Value transfer delta

Select to display the transfer rate based on a delta value.

Value transfer interval

Select to display the configured transfer interval for the value.

Value transfer rate

Select to display how often a value transfer takes place.

  • Поиск
  • Add/Remove Columns Dialog Box
  • Quick Filter
  • Bindings Overview
  • Value Transfer Settings