earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
03.12.2024

Configuring the Audibility of an Alarm in Reset State

You configure an alarm to make a sound when it is in reset state and alarm state so that the operator can hear the alarm.

To configure the audibility of an alarm in reset state
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the Presentation tab.

  3. Select Audible alert to make the alarm sound when it is triggered.

     
    action_zoom_plus_stroke
  4. Click the Save button

     
    action_zoom_plus_stroke

  5. In the computer file system, locate the file named SE.SBO.WorkStation.exe.config in the folder where WorkStation is installed.

  6. Open the SE.SBO.WorkStation.exe.config file in a text editor.

  7. On the row saying: <add key="AudibleAlertOnResetState" value="false"/> , replace the word "false" with "true" to make the alert audible when an alarm is in reset state.

     
    action_zoom_plus_stroke
  8. On the File menu, click Save to save the changes you made to the file.

  9. Restart WorkStation.

  • Alarm Functions
  • Alarms Overview
  • Configuring the Audibility of an Alarm
  • Configuring a Custom Audible Alarm Alert
  • Configuring the Flashing of an Alarm
  • Turning off a Visual and Audible Alert
  • Create Alarm Wizard – Presentation Page