earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WorkStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023
2021-07-23

Searching for Forced Values

You search for forced values to determine if the system runs normally and to reset forced values. Manually overridden I/O points are not included in the search result.

Pokaż więcej
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. Więcej informacji zawiera Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Więcej informacji zawiera Viewing an Unforced Value .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Więcej informacji zawiera Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. Więcej informacji zawiera Forced Value Indication in Function Block Graphics Viewer .

To search for forced values
  1. In WorkStation, on the Toolbar, click the Search button

     
    action_zoom_plus_stroke
    .

  2. In the Search view, in the text box, type your search.

    Uwaga

    To search for all forced values, type '*'.

  3. In the In folder box, enter the folder where you want to start the search.

  4. Select Include subservers to include automation subservers in the search.

    Uwaga

    Only subservers running EcoStruxure Building Operation BMS version 1.5 or higher are included in the search.

  5. Select Stop if more than 1000 results to limit the search to 1,000 results.

  6. Select Forced values only to search for forced values that were forced from within the EcoStruxure BMS.

  7. Select In device to include values forced from outside the EcoStruxure BMS in the search. For example, values forced on the device.

  8. In the Select Types dialog box, in the Include types box, select object types to include in your search.

  9. Click the Add type button

     
    action_zoom_plus_stroke
    .

  10. Click OK .

  11. In the Select Conditions box, enter the search conditions that have to be met before a search result is displayed.

  12. Click the Add condition button

     
    action_zoom_plus_stroke
    and select the condition you want to use for the search.

  13. Click OK .

  14. Click the Search button

     
    action_zoom_plus_stroke
    .

The forced values in the EcoStruxure BMS are displayed.

  • Search
  • Search Overview
  • Forced Values
  • Search View
  • Search View Toolbar