earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation, Project Configuration Server
功能: 基本功能
产品版本: 1.8
2016/6/10

Searching for Forced Values

You search for forced values to determine if the system runs normally and to reset forced values. Manually overridden I/O points are not included in the search result.

显示更多
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

A forced value can be released at any time. When you release a forced value, the value returns to its normal status.

A forced value is indicated by orange color in the properties dialog boxes. In the List View and in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

You can view the unforced value, which is the real value from the system, at any time. 有关更多信息,请参阅 浏览非强制值 .

The forced values in the Building Operation system are displayed.

To search for forced values
  1. In WorkStation, on the Toolbar, click the Search button

     
    action_zoom_plus_stroke
    .

  2. In the text box, type your search.

    注释:

    To search for all forced values, type '*'.

  3. In the In folder box, select the folder where you want to start the search.

  4. Expand Advanced settings .

     
    action_zoom_plus_stroke
  5. Select Include subservers to include SmartStruxure subserver devices in the search.

    注释:

    Only subservers running Building Operation version 1.5 or higher are included in the search.

  6. Select Stop if more than 1000 results to limit the search to 1,000 results.

  7. Select Forced values only to search for forced values.

     
    action_zoom_plus_stroke
  8. In the Include types box, click the browse button

     
    action_zoom_plus_stroke
    to include a specified object type in your search.

     
    action_zoom_plus_stroke
  9. Select the object types you want to include in the search and then click the Add type button

     
    action_zoom_plus_stroke
    .

  10. Click OK .

  11. In the Select Conditions box, click the browse button

     
    action_zoom_plus_stroke
    to select a condition for the search.

     
    action_zoom_plus_stroke
  12. Click the Add condition button

     
    action_zoom_plus_stroke
    and select the condition you want to use for the search.

  13. Click OK .

  14. Click the Search button

     
    action_zoom_plus_stroke
    .

  • Advanced Search
  • Search Overview
  • Forced Values