earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Removing Attachments from Multiple Alarms

You remove all alarm attachments, for example, .pdf files or a trend logs that are no longer relevant for assisting you when diagnosing or solving the problem that caused an alarm.

显示更多
action_close

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

附件还可以是:包含有关报警信息的语音消息、报告、趋势图、时间表、Microsoft Word 文件、PDF 文件、视频录制或弹出窗口。

您可以通过单次操作为多个报警添加相同的附件或附件集。还可以通过单次操作删除属于多个报警的附件。如果要添加的附件已附加到某个报警,则后续附件会作为重复项添加。

您可以打开附件,前提是与附件关联的程序或编辑器已本地安装在您的计算机上。例如,如果附件是 PDF 文件,而您的计算机上已安装 Adobe Reader 或类似程序,则可以打开此文件。

To remove attachments from multiple alarms
  1. In WorkStation, in the list view, select the alarms from which you want to remove all alarm attachments.

  2. On the Actions menu, point to Advanced and then click Remove all attachments .

  3. In the Remove all Attachments dialog box, click Yes .

All alarm attachments are removed from the selected alarms.

  • 报警附件
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Copying Attachments to Multiple Alarms
  • Removing an Attachment from an Alarm